Normalize IQ Traces
When is selected, the VSA normalizes or scales the demodulated trace data results to the IQ Reference signal power. For more information about Normalization, see IQ Normalize (Digital Demodulation).
The IQ trace data results (including IQ Meas, IQ Ref, Error Vect vs. Sym, and Error Vect vs. Carrier) are normalized.
The IQ trace data results are not normalized.
When normalization is selected and the trace is a vector or constellation diagram, the VSA markers are cross-hairs or circles at the ideal constellation locations
See Also
Custom OFDM Demodulation Properties Dialog Box