Advanced Tab (Custom OFDM)
The Advanced tab of the Custom OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. Demodulation Properties dialog box lets you access advanced parameters you can use to demodulate user defined and/or nonstandard OFDM signals and to manipulate trace data results.
The Component Carrier drop-down and diagram at the top of this tab help you control the component carriers to which you apply these settings.
The Advanced tab dialog box allows you to configure these parameters:
- Advanced
- Ant. Det. Threshold
- Compensate Symbol Clock Error
- DFT-S-OFDM Err Vector Traces
- EVM Normalized by Reference
- Extended Frequency Lock Range
- Extended Frequency Lock Range Width
- Mirror Frequency Spectrum
- Per-Symbol Phase Compensation Frequency Mode
- Per-Symbol Phase Compensation Manual Frequency
- Reference Symbol Mode
- Symbol Time Adjustment
- Synchronization Antenna Port
- Synchronization Channel Index
- Synchronization Mode
- Advanced Display
- Advanced Synchronization Region
- Reference Subcarrier Symbols
See Also