Load Resource Allocations (CCn) (Custom OFDM)
The button opens a dialog to load a "*.csv" formatted text file that contains an array containing the allocation ID value mapped to each subcarrier and symbol OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. Resource Unit (RU RU is an abbreviation for Resource Unit, where one resource unit is a single subcarrier at a single symbol time. The value displayed is the total number of resource units occupied by subcarriers of the specified Resource Type.) in the signal. The values are loaded into the Resource Allocations parameter text box.
Load Resource Allocations acts on the component carrier scope chosen with the Component Carrier control at the top of the tab. The button caption shows the scope it will act on:
-
Load Resource Allocations (CCn) — an individual component carrier is selected, and only that carrier is configured. The other component carriers are unchanged.
-
Load Resource Allocations (All CC) — all component carriers are selected, and every component carrier is configured.
See Also