Format Tab (Custom OFDM)

The Format tab of the Custom OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. Demodulation Properties dialog box lets you configure the demodulator for Custom OFDM signals. These are the parameters necessary for the VSA to lock on to and demodulate the test signal.

The Component Carrier drop-down and diagram at the top of this tab help you control the component carriers to which you apply these settings.

The Format tab dialog box enables you to configure these buttons and parameters:

Frame Parameters

General

Time Domain

Frequency Domain

Frame Diagram

Allocations & Frame Parts

Allocations

Allocations: Per Frame Part

Allocations: Per Allocation

Allocations: Per User

See Also

See "Component Carrier Selection (Custom OFDM)"

Custom OFDM Demod Properties Dialog Box