Load Resource Map (CCn) (Custom OFDM)
The button opens a dialog to load a "*.csv" formatted text file that contains an array of the Type of "Resource" for each used subcarrier and symbol time in the measurement. The resource type values are loaded into the Resource Map parameter text box.
Load Resource Map acts on the component carrier scope chosen with the Component Carrier control at the top of the tab. The button caption shows the scope it will act on:
-
Load Resource Map (CCn) — an individual component carrier is selected, and only that carrier is configured. The other component carriers are unchanged.
-
Load Resource Map (All CC) — all component carriers are selected, and every component carrier is configured.
See Also