Load Resource Modulation (CCn) (Custom OFDM)

The Load Resource Modulation (CCn)... button opens a dialog to load a "*.csv" formatted text file that contains an array of the "Modulation" type for each used resource "used subcarrier and symbol time" in the measurement.  The values are loaded into the Resource Modulation parameter text box.

Load Resource Modulation acts on the component carrier scope chosen with the Component Carrier control at the top of the tab. The button caption shows the scope it will act on:

See Also

Format Tab

Custom OFDM Demod Properties