Ant. Det. Threshold (Custom OFDM)
sets the power threshold in dB relative to the max power of all available MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. paths used for detecting whether an antenna port is active on an input channel for this PDSCH Physical Downlink Shared Channel.
Default: -36 dB
See Also