Menu Path: Analysis > Custom OFDM Demod Properties > Advanced tab
The Extended Frequency Lock Range Width parameter specifies the number of subcarriers used to extend the VSA frequency lock range when Extended Frequency Lock Range is selected.
See Extended Frequency Lock Range for more information.
See Also
Advanced Tab (Custom OFDM)
Custom OFDM Demod Properties
Copyright © 2000-2026 Keysight Technologies, Inc.