Mirror Frequency Spectrum (Custom OFDM)

Mirror Frequency Spectrum allows time domain conjugation, which mirrors the frequency-domain around the center frequency. Mirror Frequency Spectrum allows you to correctly demodulate frequency spectrums that are mirrored (flipped) about the center frequency. The default frequency spectrum is not mirrored. This parameter does not change the displayed spectrum trace data.

Cleared: Does not mirror the frequency spectrum.

Selected: Mirrors the frequency spectrum about the measurement hardware's center frequency.

The display of the spectrum data will not change with this parameter. To mirror the display, clear the Mirror Frequency Spectrum check box here and select Analysis > Frequency > Frequency tab > Mirror Frequency check box.

See Also

Advanced Tab (Custom OFDM)

Custom OFDM Demod Properties