Per-Symbol Phase Compensation Manual Frequency (Custom OFDM)
1 GHz Gigahertz: A frequency measurement which equals one billion hertz.
sets the frequency used for symbol phase compensation of the signal under test when Per-Symbol Phase Compensation Frequency Mode is set to Manual.
See Also