Advanced Synchronization Region Properties (Custom OFDM)
When Synchronization Region Selection is set to , the Synchronization Region properties allow you to customize the synchronization of the measured signal with the reference signal. The available Synchronization Region properties are:
| Parameters | Designs |
|---|---|
|
Sets the interval of the reference signal to use for synchronization. This property can be used with Synchronization Reference Offset to precisely define the reference signal used for synchronization, which can speed up measurement processing, or provide more robustness for certain measurements. Default: 10 Symbols |
|
|
Sets the offset of the reference signal to use for synchronization. This property can be used with Synchronization Reference Interval to precisely define the reference signal used for synchronization, which can speed up measurement processing, or provide more robustness for certain measurements. Default: 0 Symbols |
|
|
Sets the synchronization search interval (in symbols) used when synchronizing to the signal. This property can be used with Synchronization Search Offset to reduce the search region for synchronization, which can speed up measurement processing, or provide more robustness for certain measurements. Default: 10 Symbols |
|
|
Sets the synchronization search offset (in symbols) used when synchronizing to the signal. This property can be used with Synchronization Search Interval to reduce the search region for synchronization, which can speed up measurement processing, or provide more robustness for certain measurements. Default: 0 Symbols |
See Also