Equalizer & Tracking Tab (Custom OFDM)
The Advanced tab of the Custom OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. Demod Properties dialog box lets you access advanced parameters you can use to demodulate user defined and/or nonstandard OFDM signals and to manipulate trace data results.
The Advanced tab dialog box allows you configure these parameters:
- Equalizer (Training)
- Equalizer: Details
- Tracking
See Also