Power Boost Level Per Allocation (Custom OFDM)

Menu Path: Analysis > Custom OFDM Demodulation Properties > Format tab

This property is only valid when Resource Interface = Type2.

Power Boost Level Per Allocation is an array describing the power boost level associated with each allocation ID, as listed in the Resource Allocations mapping array.

This property is an array of values, with one value for each allocation ID, as listed in the Resource Allocations mapping array. The values are unitless. A value of 1 means no power boosting, while a value of 2 means there is a 6.02 dB power boost for the user ID. If this array is shorter than the highest allocation ID, any values past the end are assumed to be 1.

See Also

Format Tab

Custom OFDM Demod Properties