Frame Part ID Per Allocation (Custom OFDM)

Menu Path: Analysis > Custom OFDM Demodulation Properties > Format tab

This property is only valid when Resource Interface = Type2.

Frame Part ID Per Allocation is an array describing the frame part ID associated with each allocation ID, as listed in the Resource Allocations mapping array.

This property is an array of values, with one value for each allocation ID, as listed in the Resource Allocations mapping array. The values are unitless. The frame part ID value can be used to index into the per FramePart array properties to extract associated configuration settings. If this array is shorter than the highest allocation ID, any values past the end are assumed to be 0.

See Also

Format Tab

Custom OFDM Demod Properties