Resource Type Per Allocation (Custom OFDM)

Menu Path: MeasSetup > Custom OFDM Demodulation Properties > Format tab

This property is only valid when Resource Interface = Type2.

Resource Type Resurce Type specifies the function of the measurement subcarriers; preamble, pilot, data, All, UserN, Unknown, or Null subcarrier Per Allocation is an array describing the resource subcarrier type associated with each allocation ID, as listed in the Resource Allocations mapping array.

This property is an array of values, with one value for each allocation ID, as listed in the Resource Allocations mapping array. The values are unitless. The resource type value can be used to determine the type of subcarrier for each allocation. The valid range of resource type values are 0 = Data, 1 = Pilot, 2 = Unknown Pilot, 3 = Preamble, 4 = Idle, 5 = Unspecified, 6 = Known Data. If this array is shorter than the highest allocation ID, any values past the end are assumed to be 0 (Data).

See Also

Format Tab

Custom OFDM Demod Properties