Guard Interval Repeat Index (Custom OFDM)

Menu Path: Analysis > Custom OFDM Demodulation Properties > Format tab

Default: 0

Guard Interval Repeat Index - If the Guard Interval Per Symbol array is at least as long as the measurement result length, it provides a guard interval value for each symbol. If the array is shorter than the measurement result length, processing loops back and re-uses the array (and keeps looping back every time the end of the array is reached again). The location within the array that is looped back to is determined by the Guard Interval Repeat Index. For clarity in the explanation below, let RepeatIndex equal the Guard Interval Repeat Index, and ArrayLength equal the length of the Guard Interval Per Symbol array. There are four possible cases:

See Also

Guard Interval Per Symbol

Format Tab

Custom OFDM Demod Properties