Name Per User (Custom OFDM)
is a comma-separated list of names for each user. If the number of names is not enough, any names past the end are constructed automatically. The default value is an empty string (which means that all user names are constructed automatically).
See Also