MIMO Analysis (Custom OFDM)
MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. Analysis contains parameters that specify the allocation's antenna port mapping definitions.
- Determines whether this allocation is mapped to multiple (i.e. all) active antenna port indexes or not.
This setting value is only available when the allocation Type is set to either Data or Idle.
This setting value will be ignored when the allocation Type is set to either Pilot or Preamble.
Selected (default) - The allocation is mapped to multiple (i.e. all) active antenna port indexes.
Cleared - The allocation is mapped to only the individual antenna port index specified by the Antenna Index parameter.
- Sets the individual antenna port index to which the allocation is mapped.
This setting is required if the allocation Type is set to either Pilot or Preamble. It is also required if the allocation Type is set to either Data or Idle when Multiple Antenna is set to false.
Default: 0
See Also