Frame Definition Tab (Custom OFDM)
The tab of the configures the frame's general settings, frame parts and allocations.
The Component Carrier drop-down and diagram at the top of this tab help you control the component carriers to which you apply these settings.
The Frame Definition tab contains these parameters:
Preset to Standard (CCn) - Configures the VSA to measure one of several signals based on the 5G NR and 6GR standards. You can also use Format > Preset to Standard (CCn) to configure several other standard formats in addition to 5G NR and 6GR signals.
Frame Parameters
General tab
Time Domain tab
- System Rate
- Cyclic Prefix (Ratio) Per Symbol
- Cyclic Suffix (Ratio) Per Symbol
- CP/CS Repeat Index
- Signal is Bursted
- Time Gap (Samples) Per Symbol
- Time Gap Repeat Index
- Transmitter Window Beta (Ratio)
- Resource Map Length
- Resource Map Repeat Index
Freq Domain tab
Allocation Summary
- Index
- Enabled
- Frame Part
- Allocation
- User Name
- Type
- Power
- Sequence
- Custom Seq
- Modulation
- Symbols
- Subcarriers
- Ports
Frame Parts
Frame Part Parameters
Channel Estimation CDM Group
Allocation Parameters
Configuration
Payload
Location
MIMO Configuration
- Active Port (Pilot/Preamble)
- Active Ports (Data/Idle)
See Also
See "Component Carrier Selection (Custom OFDM)"
Custom OFDM Demod Properties Dialog Box