Selecting the Custom OFDM Demodulator

(option BHF only)

Select the CustomOFDM measurement type to set the VSA to demodulate and analyze Custom OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. formatted signals.

Configure the Demodulator

After selecting the demodulator, you must configure the demodulator to measure your Custom OFDM signal. Open the Custom OFDM Demod Properties dialog (Menu Path: Analysis > Custom OFDM Demodulation Properties ....) to configure the Custom OFDM signal parameters.

For a review of OFDM modulation, see OFDM Overview.

Example recordings

The 89600 VSA includes several examples in the ...\Signals\CustomOfdm folder that can be used to help you learn how to use the Custom OFDM demodulator. The included signals are listed in the Demo and Recorded Signals topic in the Getting Started book.

See Also

Custom OFDM Demodulation Properties Dialog Box