Result Length Selection (Custom OFDM)
The parameter is used to specify the measurement analysis data, see Time trace. There are two Result Length modes; or mode. In general, "Automatic" mode will limit the measurement result length and Measurement Interval to the burst length. "Manual" mode will allow the measurement result length and measurement interval to include data beyond the burst length.
|
In Automatic mode the VSA automatically determines the correct measurement result length and protects against including non-burst data in the measurement analysis. There are two Automatic mode Result Length conditions: 1) Result Length > Burst Length: 2) Result Length ≤ Burst Length |
|
| The VSA uses the specified Result Length as the maximum Result Length. All input data specified by the and parameters will be included in the measurement analysis even if the specified Measurement Interval includes data beyond the measurement burst. |
Example: The following figures show the difference between Automatic and Manual modes when the Results Length is greater than the first measurement burst.
See Also