Time Tab (Custom OFDM)
The Time tab of the Custom OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. Demodulation Properties dialog box lets you access the signal capture configuration parameters. You use these parameters to select the pulse search length and to isolate a segment of the time record for further viewing and data analysis.
The Component Carrier drop-down and diagram at the top of this tab help you control the component carriers to which you apply these settings.
The Time tab dialog box allows you to configure these parameters:
Time
Time:Details
See Also