Default Anchor State (Digital Demod)
The parameter determines the assumed value for the first bit from the differential decoder. It is only available when Format is MSK Minimum Shift Keying Type 1 and Constellation Sync Search is not active.
There are two possible modes:
- : The assumed value for the first bit from the differential decoder is 0.
- (default): The assumed value for the first bit from the differential decoder is 1.
See Also