Advanced Tab (Digital Demod)
The specifies parameters specific to certain demodulation formats.
The parameters are:
- APSK Ring Ratios
- Star-QAM Quadrature Amplitude Modulation Ring Ratios (only available when Format is Star 16-QAM or Star 32-QAM)
- CPM Auto {h1,h2}
- Low SNR Enhancement
- Default Anchor State (only available when Format is MSK Minimum Shift Keying Type 1 and Constellation Sync Search is not active)
- Shaped OQPSK Offset Quadrature Phase Shift Keying: A type of QPSK modulation that offsets the bit streams on the I and Q channels by a half bit. This reduces amplitude fluctuations and helps improve spectral efficiency. Parameters
See Also