Search Time (Digital Demod)
When is enabled and Pulse Search or Constellation Sync Search is ON, the trace shows time-data before and digital demodulation, as shown in the following block diagram. The value of Search Length determines the length of the trace.
This trace is only available when or is on.
This trace displays the acquired input time data which the demodulator searches for the burst.
The following block diagram is part of the Digital Demodulation Block Diagram.