Time (Digital Demod)
When is enabled, the trace shows the time record before digital demodulation and after pulse search, as shown in the following block diagram. (The block diagram is part of the Digital Demodulation Block Diagram).
The trace has the following characteristics:
- Unaffected by time averaging
- Is 20% longer than the since the trace displays the data before demodulation. The trace shows 10% of
the before the demodulated segment and 10% after.
For example, in the following illustration, only the section between the first and last grid lines (x-axis) is demodulated.