DOCSIS 4.0 Downstream Demod Properties Dialog Box

The DOCSIS 4.0 Downstream Demod Properties dialog box contains parameters that let you configure the VSA to demodulate user defined DOCSIS 4.0 Downstream modulated signals.

The DOCSIS 4.0 Downstream demodulator must be selected before this dialog box is available. To enable the demodulator, click Analysis > Measurement Type > Other standard formats > DOCSIS 4.0 Downstream.

The dialog box contains these tabs:

See Also

Selecting the DOCSIS 4.0 Downstream Demodulator

Making a DOCSIS 4.0 Downstream Measurement