OFDM Inst Eq Ch Freq Resp(DOCSIS 4.0 Downstream)
The trace is the non-averaged Ch Frequency Response trace data for the specified measurement hardware. If averaging is selected, the Inst Ch Frequency Response does not show the effects of averaging; however, it is affected by equalizer smoothing selection on the Equalizer & Tracking tab.
If averaging is off, the Inst Ch Frequency Response trace is identical to the Ch Frequency Response trace, including the trace title.
See Also