Burst Description (DOCSIS 4.0 Upstream)
reports the current Burst Minislot Configuration per allocation. If Auto Detect MiniSlot Start and Length is enabled, the Burst Description metric shows the detected values. If Auto Detect is disabled, the manually specified values are displayed.
| Alloc0 | AllocN | ||||||
|---|---|---|---|---|---|---|---|
| [MiniSlot Start | MiniSlot End* | Pilot Pattern | Bit Loading] | [MiniSlot Start | MiniSlot End* | Pilot Pattern | Bit Loading] |
* MiniSlot End = (MiniSlot Start + MiniSlot Length - 1)
A displayed value of "***" means no data is available.
See Also
Available Error Summary Results