Excluded Subcarriers (DOCSIS 4.0 Upstream)
reports the current Excluded/Unused/Guard Band Configuration per exclusion band. If Auto Detect is enabled, the Excluded Subcarriers metric shows the detected values. If Auto Detect is disabled, the manually specified values are displayed.
| Exc0 | Exc1 | ExcN | |||
|---|---|---|---|---|---|
| [Subcar Start | Subcar End*] | [Subcar Start | Subcar End*] | [Subcar Start | Subcar End*] |
* Subcar End = (Subcar Start + Subcar Length - 1)
A displayed value of "***" means no data is available.
See Also
Available Error Summary Results