RLE Status (DVB-RCS2)
There are two types of traces in the Trace > Data > Demod menu that display component carrier data: CCn (component carrier is fixed), and Display CC (component carrier is dynamically selected using the Carrier Aggregation > Selected CC for Trace Display parameter). See About Demod Per-Carrier Trace Types for more information.
The trace shows the SDUs recovered from the frame(s) plus summary counters for decode problems, so you can see what was decapsulated and diagnose failures. For DVB-RCS2, RLE (Return Link Encapsulation) decapsulation runs automatically on traffic bursts.
RLE Status is a type of Matrix Table that provides selectable column visibility and copy/paste and export functionality to share rows of content or complete tables to applications like email, text editing or spreadsheet programs.
Four aggregate counters are shown above the RLE Status table:
-
Total SDUs — Number of RLE SDUs found in the frame(s).
-
Fragmented SDUs — Count of SDUs whose ALPDU was carried in more than one PPDU 1) IEEE 802.11: PHY (formerly PLCP) protocol data unit or 2) DVB-RCS2 (RLE): payload adapted PDU (start, continuation, and end fragments), including reassemblies that did not complete or that failed their integrity check. Compare with Total SDUs to see how many SDUs arrived unfragmented.
-
Frame CRC Cyclic Redundancy Check Failures — Count of Frame PDU (protocol data unit) The data unit exchanged between peer entities of the same protocol layer. On the downward direction, it is the data unit generated for the next lower layer. On the upward direction, it is the data unit received from the previous lower layer. CRC failures.
-
ALPDU Integrity Failures — Count of reassembled SDUs whose trailer (CRC-32 or sequence number) failed.
The RLE Status table has one row per SDU:
| SDU # | Integrity | Fragment ID | Fragments | Offset (bit) | Length (bit) | First Frame | Last Frame | Protocol Type | Label Type | Payload Label |
|---|---|---|---|---|---|---|---|---|---|---|
|
SDU index within the result. |
Decode status of the SDU:
|
RLE fragment id (reassembly key, 0–7) tying this SDU's row to its fragments. *** for a full (unfragmented) SDU and for signaling frames, which have no fragment id. |
Number of fragments the SDU was reassembled from. |
Bit offset of the SDU within the decapsulated stream (Meas BER Bit Error Ratio - A ratio of the number of errors to data bits received on a digital circuit. Bits). *** on rows that recover no payload. |
SDU length, in bits. *** on rows that recover no payload. |
Index of the first frame in which a fragment of this SDU was seen. | Index of the last frame in which a fragment of this SDU was seen. |
RLE Protocol Type (hex); *** when suppressed or unknown. |
ALPDU label type (0–3); *** when unknown. |
Implicit FPDU payload label (hex), packed most-significant byte first. Decoded only when Payload Label Size is set to a nonzero value for the section. *** when the size is 0 (the default), and for label sizes of 7 bytes or more, which are shown as not applicable rather than as a truncated value. |
See Also