High Symbol Rate (GSM/EDGE/EDGE Evolution)
325 kHz kiloHertz: A radio frequency measurement (one kilohertz = one thousand cycles per second).
Min: Normal Symbol Rate
Max: 2*Normal Symbol Rate
sets the symbol rate for high symbol rate bursts (HB).
The symbol rate for normal bursts can be set using the Normal Symbol Rate parameter.
See Also