Advanced Tab (GSM/EDGE/EDGE Evolution)
The contains parameters which are used for fine tuning demodulation results or for demodulating non-standard signals.
- Normal Symbol Rate
- High Symbol Rate
- Burst Search Threshold
- IQ Constellation Type
- Measurement Filtered Only
- Meas+Complementary Filtered
- Meas+Complementary Filtered + Derotated
- Normalize IQ Traces
- Mirror Frequency Spectrum
- Wide Frequency Lock Range
- Use Multicarrier Filter
- Enable Droop Compensation
- Align Polar Modulation
See Also
GSM/EDGE/EDGE Evolution Demod Properties dialog box