Freq Err (GSM/EDGE/EDGE Evolution)
Freq Errdisplays the frequency offset of the demodulated burst from the center frequency of the VSA. The frequency offset is averaged over all symbols in the burst (shown in the Time trace).
See Also
Freq Errdisplays the frequency offset of the demodulated burst from the center frequency of the VSA. The frequency offset is averaged over all symbols in the burst (shown in the Time trace).
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |