Reference Carrier (Flex Frame)
sets the carrier to be used as the reference carrier. The value is a zero-based index of the carrier used as the synchronization reference. Enabled only when Carrier Alignment = Reference Carrier.
See Also
sets the carrier to be used as the reference carrier. The value is a zero-based index of the carrier used as the synchronization reference. Enabled only when Carrier Alignment = Reference Carrier.
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |