Custom Modulations (Flex Frame)

Within the Custom Modulation tab, you can import, export, and edit standard-based modulation schemes as well as user-defined custom modulation schemes. You can also create a custom modulation directly in the VSA.

The Custom Modulation tab is used when an allocation's Modulation is set to Custom Modulation.

Constellation Mapping

Custom Modulation Editor

When you click a custom modulation, the selected modulation's constellation is displayed in the Constellation Table.

Constellation Table

Edit- When clicked, the parameters in the constellation table become editable, and several controls are added to customize the modulation. Any edited states must align with the selected modulation format, in order to create a constellation that is valid.

Constellation Editor

When you manually edit constellation points (IQ values, magnitude/phase, or adding/removing states) in the Custom Modulation Editor, the Modulation dropdown automatically switches to "UserDefined".

See Also

Custom Modulation Tab