Configuration (Allocation) (Flex Frame)
Configuration contains parameters that specify the allocation's name, type, power boost and payload.
enables or disables the analysis of an allocation. At least one is always enabled. If you try to disable all of them, the first allocation will be automatically enabled.
sets name of the selected allocation (limited to 30 characters).
selects the allocation type.
- Preamble- configures the allocation as a preamble. Preamble allocations are used for initial sync and channel estimation.
- Data- configures the allocation as data. Data allocations carry data payload.
- Pilot- configures the allocation as a pilot. Pilot allocations are typically interspersed within the data and are used for tracking and updating channel estimation.
- Idle- configures the allocation as idle. Idle allocations are the off, or ignored, portion of the frame.
Default: Data
Range: Preamble, Data, Pilot, Idle
sets the relative power boosting (dB) of this allocation relative to the other allocations.
All constellations are normalized to the same RMS power, so absolute power of the 0 dB level is set to the measured RMS average of all allocations whose PowerBoostLevel is 0 dB.
Default: 0
Payload - These parameters define the allocation's payload:
specifies the allocation's PN 1) part number, or 2) packet number sequence. See About PN Sequence Generation for more information.
- Unknown - specifies that the payload is unknown (known modulation).
- PN9 - specifies a PN9 bit sequence, as specified in CCITT T-REC-O.153.
- PN11 - specifies a PN11 bit sequence, as specified in CCITT T-REC-O.153.
- PN15 - specifies a PN15 bit sequence, as specified in CCITT T-REC-O.151.
- PN20 - specifies a PN20 bit sequence, as specified in CCITT T-REC-O.153.
- PN23 - specifies a PN23 bit sequence, as specified in CCITT T-REC-O.151.
- Custom - specifies a custom sequence.
Default: PN23
Choices: Unknown, PN9, PN11, PN15, PN20, PN23, Custom
specifies the type of custom sequence when Sequence is set to Custom. After selecting the Custom Sequence Type, enter or paste the sequence into the field below the Modulation parameter. Be sure the entered data matches the specified type.
- Bit Sequence- Bit Sequence is a list of digits with no space between.
- IQ Symbol Sequence- IQ Symbol Sequence is a comma-separated list of interleaved real and imaginary values, representing the IQ symbols in the allocation payload.
selects the allocation's modulation format.
- BPSK Binary phase shift keying - A type of phase modulation using 2 distinct carrier phases to signal ones and zeros.- the allocation uses a BPSK modulation format.
- QPSK Quadrature phase shift keying- the allocation uses a QPSK modulation format.
- 8-PSK Phase Shift Keying: A broad classification of modulation techniques where the information to be transmitted is contained in the phase of the carrier wave.- the allocation uses an 8-PSK modulation format.
- 16-QAM Quadrature Amplitude Modulation- the allocation uses a 16-QAM modulation format.
- 32-QAM- the allocation uses a 32-QAM modulation format.
- 64-QAM- the allocation uses a 64-QAM modulation format.
- 128-QAM- the allocation uses a 128-QAM modulation format.
- 256-QAM- the allocation uses a 256-QAM modulation format.
- 512-QAM- the allocation uses a 512-QAM modulation format.
- 1024-QAM- the allocation uses a 1024-QAM modulation format.
- 2048-QAM- the allocation uses a 2048-QAM modulation format.
- 4096-QAM- the allocation uses a 4096-QAM modulation format.
- 8192-QAM- the allocation uses a 8192-QAM modulation format.
- 16384-QAM- the allocation uses a 16384-QAM modulation format.
- 32768-QAM- the allocation uses a 32768-QAM modulation format.
- DVB-S2/S2X APSK- the allocation uses a DVB-S2/S2X APSK modulation format. When selected, use the MODCOD parameter to select the appropriate modulation.
- DVB-S2/S2X ϖ/2 BPSK- the allocation uses a DVB-S2/S2X ϖ/2 BPSK modulation format.
- Custom - the allocation uses a custom imported modulation format. Use Import... to import a custom modulation format. Imported modulation formats will be added to the Custom Name drop-down list to select a custom modulation format.
Default: BPSK
Choices: BPSK, QPSK, 8-PSK, 16-QAM, 32-QAM, 64-QAM, 128-QAM, 256-QAM, 512-QAM, 1024-QAM, 2048-QAM, 4096-QAM, 8192-QAM, 16384-QAM, 32768-QAM, DVB-S2/S2X APSK, DVB-S2/S2X ϖ/2 BPSK, Custom
(when Modulation is set to Custom Modulation) provides a drop-down list of custom modulation formats imported using the Import... parameter.
(when Modulation is set to Custom Modulation) opens a dialog to import a custom modulation format. Imported modulation formats will be added to the Custom Name drop-down list to select a custom modulation format.
The same Import functionality is available in the Custom Modulation tab, which also provides constellation summaries and a means of managing and exporting custom modulations.
(when Modulation is set to DVB-S2/S2X APSK) selects the S2X APSK modulation as specified in Table 17a of the ETSI European Telecommunications Standard Institute: The European standardization body for telecommunications. EN 302 307-2 V1.2.1 (2020-08) standard document.
- 2+4+2APSK Normal 100/180
- 2+4+2APSK Normal 104/180
- 8+8APSK Normal 90/180
- 8+8APSK Normal 96/180
- 8+8APSK Normal 100/180
- 4+12APSK Normal 26/45
- 4+12APSK Normal 3/5
- 8+8APSK Normal 18/30
- 4+12APSK Normal 28/45
- 4+12APSK Normal 23/36
- 8+8APSK Normal 20/30
- 4+12APSK Normal 25/36
- 4+12APSK Normal 13/18
- 4+12APSK Normal 140/180
- 4+12APSK Normal 154/180
- 4+12+16rbAPSK Normal 2/3
- 4+8+4+16APSK Normal 128/180
- 4+8+4+16APSK Normal 132/180
- 4+8+4+16APSK Normal 140/180
- 16+16+16+16APSK Normal 128/180
- 4+12+20+28APSK Normal 132/180
- 8+16+20+20APSK Normal 7/9
- 8+16+20+20APSK Normal 4/5
- 8+16+20+20APSK Normal 5/6
- 128APSK Normal 135/180
- 128APSK Normal 140/180
- 256APSK Normal 116/180
- 256APSK Normal 20/30
- 256APSK Normal 124/180
- 256APSK Normal 128/180
- 256APSK Normal 22/30
- 256APSK Normal 135/180
- 4+12APSK Short 7/15
- 4+12APSK Short 8/15
- 4+12APSK Short 26/45
- 4+12APSK Short 3/5
- 4+12APSK Short 32/45
- 4+12+16rbAPSK Short 2/3
- 4+12+16rbAPSK Short 32/45
Default: 128APSK Normal 135/180
determines whether the allocation's payload sequence restarts in each frame or continues from one frame to the next. It applies when the payload sequence is a PN type or a custom bit sequence.
- Reset At Each Frame - each frame re-reads the payload sequence from its start.
- Continuous Over Frames - the payload sequence is consumed continuously, so each frame picks up the sequence where the previous frame left off.
Set this to Continuous Over Frames when the transmitter sends one uninterrupted sequence and the Result Length spans more than one frame. Left at Reset At Each Frame, the reference sequence restarts at every frame boundary while the transmitted sequence does not, so bit errors appear in every frame after the first.
Default: Reset At Each Frame
Choices: Reset At Each Frame, Continuous Over Frames
determines whether the allocation is included in Bit Errors, Bit Count and BER Bit Error Ratio - A ratio of the number of errors to data bits received on a digital circuit. metrics. See Frame Summary, Carrier Summary and Syms/Errs for more information.
An allocation supports BER calculations if the allocation's payload sequence is either a PN type or a custom bit sequence (Sequence = Custom and Custom Sequence Type = Bit Sequence).
You can also include/exclude BER calculations for each allocation using Measurement Control > Overall Allocation Control > Calculate BER.
determines where the allocation's payload sequence is assumed to begin.
Default: Cleared
- Cleared - the payload sequence is assumed to begin at the allocation's first symbol (Start Symbol).
- Selected - the demodulator searches the received bits for the start of the payload sequence and uses the best match as the BER reference.
Select this check box whenever the transmitted sequence runs continuously and its phase is not aligned to the frame - a free-running PN generator, for example. Such a sequence is at an arbitrary point when the acquisition starts, so with the check box cleared the reference never matches the signal. Synchronization then fails and every value in the error summary becomes invalid, not just BER. The status reported in that case is "No sync pattern present or search length too short", but the search length is not the problem. See Measuring BER on a Continuously Transmitted Sequence.
Autodetect Bit Sequence Offset is visible when the allocation's payload sequence is either a PN type or a custom bit sequence (Sequence = Custom and Custom Sequence Type = Bit Sequence), and available when Include in BER Calculations is selected. It has no effect on an unknown payload or on a custom IQ symbol sequence.
An allocation whose bit sequence offset is autodetected cannot also be used for synchronization, because its bits are not known until the offset has been found. Selecting this check box therefore removes the allocation as a Synchronization source, and Synchronization cannot be selected for that allocation while the check box remains selected. A synchronization allocation is not required: when the frame contains no known sequence, the demodulator synchronizes using the generic characteristics of the signal's modulation format. See About Synchronization.
In a frame that contains only one allocation, the autodetected sequence cannot also serve as the phase reference, so the demodulator assumes one of the carrier phase rotations permitted by the modulation format. If the assumed rotation is not the transmitted one, the recovered bits are wrong and BER remains high regardless of signal quality. A frame that contains more than one allocation does not have this restriction - BER is calculated for the allocations that are not used for synchronization.
Scrambling - These parameters configure scrambling applied to the allocation.
determines whether scrambling is enabled for the allocation.
(when scrambling is enabled) selects the scrambler to be used by the allocation.
Default: 0
Range: 0 - (depends on the number of configured scramblers)
See Also