Reference Filter (Flex Frame)
Menu Path:
Measurement Filter and the pulse-shaping filter applied by the transmitter (for example, = Raised Cosine and =Root-raised Cosine). The available Measurement Filter selections are:
specifies the filter to apply to the reference signal that is created based on the input signal. The reference filter chosen is usually a combination of theThe value of the filter is specified by the value entered in Alpha / BT.
The filtered reference time signal is shown in the IQ Ref Time trace.
See About Filters for more information.
See Also