Filter Tab (Flex Frame)
The
tab of the configures the filters used by the VSA's Flex Frame feature. This includes both a measurement filter (applied to the received signal before demodulation) and reference filter (applied to the ideal symbols after demodulation, to create the IQ Ref data).The filter settings are applied to either a single carrier or to all carriers, depending on the Component Carrier Selection. Use the Component Carrier drop-down or the Component Carrier Diagram at the top of the tab to switch between component carriers.
The Filter tab configures these parameters:
See Also
Flex Frame Properties Dialog Box