Allocation Summary (Flex Frame)
The Allocation Summary grid lists details about the configured frame allocations.
indicates the priority of the allocation. Lower numbers indicate higher priority (0 is highest). You can adjust the priority of an allocation by clicking one of the Move buttons to the right of the Allocation Summary list.
enables or disables the analysis of an allocation. At least one is always enabled. If you try to disable all of them, the first allocation will be automatically enabled.
Indicates the allocation's frame part.
Indicates the allocation's Name.
Indicates the symbols that are assigned per allocation. Symbol assignments are determined by the Location parameters and the index of the allocation. If two allocations overlap, the symbol is assigned to the allocation with the lower index.
Indicates the total number of symbols assigned to the allocation. The total is calculated based on the settings in the Location group of parameters.
See Also