Frame Definition Tab (Flex Frame - Advanced Mode)
The tab of the configures the frame definition for each component carrier.
The frame definition settings are applied to either a single carrier or to all carriers, depending on the Component Carrier Selection. Use the Component Carrier drop-down or the Component Carrier Diagram at the top of the tab to switch between component carriers. You can use the Allocations Diagram to visualize the frame definition as you build it.
The Frame Definition tab contains these parameters:
Component Carrier Configuration
See Also
Flex Frame Properties Dialog Box