Max Result Length (Flex Frame)
- When Frame Type is set to Burst and Length is set to Auto, this setting defines the maximum amount of data that will be analyzed. The frame may be shorter.
See Also
- When Frame Type is set to Burst and Length is set to Auto, this setting defines the maximum amount of data that will be analyzed. The frame may be shorter.
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |