Result Length (Flex Frame)
- When Frame Type is set to Burst and Length Auto is disabled, this setting defines the number of symbols used to compute measurement results shown in the IQ traces, Error traces, and Time trace.
See Also
- When Frame Type is set to Burst and Length Auto is disabled, this setting defines the number of symbols used to compute measurement results shown in the IQ traces, Error traces, and Time trace.
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |