Bit Count (Flex Frame)
indicates the number of bits counted for all frame allocations that are configured to be included in BER calculations.
When measurement averaging is enabled, the bit errors and bit count will accumulate until the average is reset, resulting in averaged BER Bit Error Ratio - A ratio of the number of errors to data bits received on a digital circuit. values. When measurement averaging is disabled, bit errors, bit count and BER values are reset each time a frame is repeated.
When no allocations are included in BER calculations, ‘***’ is shown.
See Also