Meas BER Bits (Flex Frame)
The trace shows only the bits from allocations that have Include in BER Calculations enabled. Compare this trace with the Ref BER Bits trace to identify where bit errors are located.
See Also
The trace shows only the bits from allocations that have Include in BER Calculations enabled. Compare this trace with the Ref BER Bits trace to identify where bit errors are located.
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |