Raw Main Time (Flex Frame)

Raw Main Time is the raw data read from the input hardware or playback file. It is similar to Time data with the following exceptions:

For the time traces (Time, Search Time, and Raw Main Time), 0 sec on the X-axis is the trigger location.

Raw Main Time data is useful in the following situations:

image\blk_RawTime_DigDemod_wmf.jpg

Marker Coupling

When marker coupling is used, markers on applicable Demod traces (e.g., Err Vect Time, IQ Meas Time, IQ Ref Time, Mag Error, Phase Error) will couple to the corresponding point on the Time, Search Time and Raw Main Time traces. For Demod traces, frame start (symbol 0) = 0 sec on the x-axis.