Highlight Selected Regions on Traces

Menu Path: Analysis > FMCW Radar Properties > Time

Default: ON

When Highlight Selected Regions on Traces is checked, the time samples associated with each of the Selected Regions are highlighted using alternate background colors within the Acquisition Time and synchronized Amplitude, Phase, FM Frequency Modulation and FM Slope time trace results (as shown below for the first 4 detected regions). Region highlighting includes display of the detected Region index value, which is also reported separately within the FMCW Region Table.