Selecting Stimulus/Response Data (Graph Settings)
At the top of the Graph Settings dialog, you can select the Stimulus (x-axis) and Response (y-axis) time data to use in the Graph trace. You can select most traces that contains time data. In addition to pre-demod time traces such as Search Time or Main Time, post-demod results, including IQ Meas Time and IQ Ref Time, are also available for selection. Registers with time data can also be chosen; however, Math Functions cannot be chosen.
By default, the check box is selected. In this case, the VSA will try to choose valid stimulus and response data based on these rules:
-
Single measurement defined
-
Single-channel instrument:
Stimulus = Register D1, Response = Ch1 Main Time
-
Multiple-channel instrument:
Stimulus = Ch1 Main Time, Response = Ch2 Main Time
-
-
Two or more measurements defined
Stimulus = First measurement's Ch1 Main Time, Response = Second measurement's Ch1 Main Time
To specify stimulus and response data manually, clear the check box.
See Also