Response Time (Graph Traces)
shows the response signal after compensation. This is the data that is plotted against the Stimulus Time data in one of the x-y Graph traces.
The time axis for this trace is determined by the Time Reference parameter.
The data in this trace may not exactly match that of the trace data selected as Response Data in the dialog due to the types of compensation enabled. However, you can set the Time Reference to to allow Marker Coupling between this trace and the original response trace (Ch2 Main Time for example).
See Also