Stimulus Time (Graph Traces)
shows the stimulus signal after compensation. This is the data that is plotted against the Response Time data in one of the x-y Graph traces.
The time axis for this trace is determined by the Time Reference parameter.
The data in this trace may not exactly match that of the trace data selected as Stimulus Data in the dialog due to the types of compensation enabled. However, you can set the Time Reference to to allow Marker Coupling between this trace and the original stimulus trace (Ch1 Main Time for example).
See Also